Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Accelerometer-Slide5

Zero-g offset is a measure of the output when no acceleration is present and is closely related to the sensor bias error. It is important to know the zero-g offset so that one can design their application to work properly in the presence of this error. It is also useful as a measure of accuracy when comparing sensor elements. Ideally the zero-g offset is zero, but in practice as seen in the table below it is in the mg range.

PTM פורסם ב: