Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Key Advantage 3: Energy Sharing Function (cont’d)

An actual energy sharing function with board temperature distribution testing results is shown on this slide. The images at the bottom of the slide show testing by changing the input voltage from 9 V to 16 V. At the high voltage input condition, the power dissipation is evenly controlled and avoids heat concentration to the LED driver IC, thanks to the energy sharing function.

PTM פורסם ב: