Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
opti relation
Another factor affecting sound pressure for fans in a chassis is the distance of the obstruction from the fan. The top curves shown here are sound pressure measurements taken for varying the distance of a faceplate from the inlet of a fan. The 10 mm distance shows the highest sound pressure, and it decreases as the L dimension increases. Oddly, the distance of a faceplate from a fan on the outlet side does not seem to make any significant effect on the sound pressure level. Therefore, selecting an optimum distance of an obstruction is an important consideration for the fan inlet.
PTM פורסם ב: