Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Operation 2
The PWM controller is also offered in a PCB type card, which allows the user to connect it to a DIN rail within a system. The PCB type controller comes in one specific control theme; either voltage, external adjustment, or thermistor control. Therefore, users need to select the appropriate control theme for their application when purchasing the PCB type controller.
PTM פורסם ב: