Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Image of Sanyo Denki Stepper Motor Basics - Pulse Command

The BS1D200P10 drive has two modes used to run the motor: the 2-input mode and 1-input mode. This determines if the designer wants to move the motor in both directions, or just in a single direction. Pulse signals are then input to determine speed and direction. All drives have different specifications on what the input values can be, for example maximum frequency, pulse signal voltage, and timing of the command pulse.

PTM פורסם ב: