Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
VLock-Slide2

SCHURTER’s new V-Lock Power Cord system provides a safe and reliable power connection. The yellow catch mechanism conveniently latches into the notched inlet or outlet to prevent accidental disconnection of the power cord from the equipment. It is also easily released by depressing the lever. The unique V-Lock Cord Retaining system not only prevents unintentional disconnection but also increases safety. The V-Lock requires no extra parts such as screw clamps or wire bails which in turn reduces assembly time resulting in a cost effective complete solution.

PTM פורסם ב: