Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Power-up the Device

The simplest way (method 1) to power-up the device is to use the 12 V / 2 A power adaptor included in the package and connect to the DC jack of ODYSSEY - X86J4105. Method 2 is to power the ODYSSEY - X86J4105 through the USB-C port with a 12 V input. Furthermore, if the monitor supports USB-PD, the customer is able to power and display ODYSSEY - X86J4105 using only one cable.

PTM פורסם ב: