Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Typical App

The diagram on this slide shows the typical application using the Si8900. In this case, the system master controller communicates with the Si8900 via a UART interface. A connection is made to the AC mains line through an inexpensive interface circuit. This circuit is made up of a dual packaged op-amp and several resistors. R1 acts as the sense resistor for current reading. The power supply for the high-voltage side of the device is derived from the mains line as well. U2 is a 3.0 V LDO that regulates power to the device and provides a bias for the interface circuitry.

PTM פורסם ב: