Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Level V and ErP Phase II Power Supplies Slide 6
Even though medical supplies are exempt from EISA or ErP efficiency requirements, SL Power has introduced new families of medical power supplies that meet level V. This chart shows the transition from level IV to V for medical supplies. It is important to note that SL Power has also increased the power offering in level V by 40%. The new MENB/MENT products are offered in wall plug and desktop with class I and Class II input models. Low leakage and meeting EMI level B are among the main attributes of these supplies.
PTM פורסם ב: