Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
SLE60SPD Series USB-PD Adapters

SL Power’s SLE60SPD series of medically approved USB-PD adapters bring commercial USB-PD technology into the medical device world. This is accomplished by ensuring that the safety and reliability needed by medical equipment manufacturers is married with the latest power technology. Available in both desktop and wall-plug versions, users have the flexibility to choose the right adapter for their end device use environment. Both models are rated at 60 Watts (3 Amps maximum) output power, are fully compliant with IEC60601-1 medical safety requirements, as well as the medical 4th edition EMC requirement needed for Home Healthcare applications. Both models also meet class B levels of conducted and radiated emissions, and include certification to the Industrial/ITE safety standards.

PTM פורסם ב: