Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Latching Form B Reed Relays Overview Slide 18

A Form B reed sensor is a normally closed reed sensor. As this presentation has shown, with a normally closed reed relay, a permanent magnet is used to close the contacts. The magnet’s size and strength are carefully chosen to ensure that the reed switch is fully closed. In this fully closed state, the contacts will remain in that state for as long as necessary. Also, the magnetic polarity must be consistent and well marked on the sensor.

PTM פורסם ב: