Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
EPP918-slide7

Once applied, during the manufacturing process, it will not migrate. It adheres to the contact instantly and remains intact without need for additional tape, mechanical barriers, or cure time – thereby eliminating the added expense that barrier methods incur. This image shows the EPP-918A has provided resistance to wear caused by repetitive mating and un-mating forces. After 2500 cycles on an untreated contact the wear on the gold can be extensive. Whereas, on the treated connector minimal damage is seen on the contacts.

PTM פורסם ב: