Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
BiCMOS to the Latest RF Product Family Slide 9

This slide shows the STW81200 performance compared to a very similar device from one of ST’s competitors. The measurement parameters in the chart at the bottom were made for an apples-to-apples comparison, highlighting the same reference frequencies, reference clock, the same PFD frequencies and etc. When doing that comparison, the STW81200’s phase noise is typically 5 to 8 dB better depending on the offset. As can be seen, ST’s 10 kHz offset at -108 dBc/Hz and 1 MHz offset at -137 dBc/Hz are quite an improvement over the competition. Also notice that ST has good spurious performance, with a couple of spurs which are lower than the many spurs of the competitor’s device, about -80 dB vs. -60 dB or worse.

PTM פורסם ב: