Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
MEMS Gyroscopes Slide 19

ST’s gyroscopes include a Self Test function. By applying a logic one to a dedicated pin, the mass is moved by an electrostatic actuator. It is then possible to detect a voltage variation on the output and verify that the mechanical mass and ASIC circuitry are working correctly. Another feature is the possibility to power down the sensor with the PD pin. When the power-down mode is activated, the calibration values remain stored inside internal registers while the rest of the circuit is turned off. The sensor consumes as little at 5 µA in the Power-Down mode.

PTM פורסם ב: