Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
LED-Slide2

An SMD LED Display is a 7-segment LED display which utilizes surface mount technology as a means of mounting on the PCB. This is in contrast to traditional 7-segment LED displays which use through-hole technology. SMD LED Displays are packaged in tape & reel, making them ready and fully compatible with pick and place automation. Being an SMD component also means that these LED display components are compatible with the lead-free reflow soldering method as opposed to wave soldering used for through-hole components. SMD LED Displays are also much more compact as compared to through-hole counterparts while being able to maintain equivalent brightness. SunLED provides a broad selection of various digit heights to support a wide range of applications. In the next several slides, this module will discuss the advantages of SMD LED Displays.

PTM פורסם ב: