Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Intro to Thin Film Chip Resistors Slide 13

Susumu also offers the RM Series Thin Film Resistor Networks, which utilize the same technology as RG series. The RM Series can be considered as multiple RG Resistors built into one chip. Because these multiple elements are processed side by side and simultaneously, the matching tolerance in resistance and TCR is unprecedented.

PTM פורסם ב: