Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
RG-Slide7

Susumu’s fine patterning capability using photolithography enables them to create resistive patterns as narrow as 10µm. For example, in order to create 2 MOhm RG3216, the designer uses relatively lower sheet resistance and a resistive pattern as narrow as 14µm. For 5 MOhm RG3216, the designer uses higher Ohms per square and 10µm pattern width.

PTM פורסם ב: