Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
tutorial previously
The tutorial previously explained how the DRAM cache and the increased overprovisioning help with sustained performance. It is equally important to offer high endurance, which means that drives can be operated for a long time in the field without need of replacement. Endurance can be measured in TeraByteWritten or Drive Writes per day. As an example, 1.9 drive writes per day for a client workload and 0.47 for the enterprise work load are very good numbers for MLC based SSDs.
PTM פורסם ב: