Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Die Cut Thermal Interface Product Offering Slide 4
When considering LED thermal management, it is critical to consider the ambient air temperature, the thermal path between LED and the heatsink, and LED efficiency. T-Global range of thermal pads addresses the critical factor of the thermal path between the LED and the heatsink. Using the correct thermal pad can significantly reduce junction temperature, which can have a profound effect on the lifetime of the LED.
PTM פורסם ב: