Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
LI Series Thermal Interface Material Slide 2

The LI series is comprised of highly thermally conductive adhesive tapes that can be used for the mechanical attachment of heat sinks and other components where thermal management is a requirement. The LI series tapes have been proven to offer excellent reliability when exposed to thermal, mechanical, and environmental conditioning. Furthermore, they are offered in a variety of configurations, as detailed in the datasheets. All products in the series are available in standard sheets, as custom die-cuts, and in rolls.

PTM פורסם ב: