Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Non-Silicone Gap Fillers Slide 6

Looking at the huge telecommunications market there are dozens of applications for T-Global materials. Five main applications are shown on this slide which can provide not only areas where non-silicones are used but the range of volumes and needs depending on the application. The traditional base station modules remain as large users of gap fillers but they also use large amounts of dispensed materials. However, this is typically used by the very large OEMs. In some of the other areas the opportunities can be just as interesting. In the bottom two pictures a standard application is shown that has rich pickings for these materials. Where there are small antennae on the digital road signs and parking systems these are typically wireless systems. Some are WiFi based, but where high power is used in the base units there is large areas of metal and heat is being generated, so there are thermal needs that require addressing.

PTM פורסם ב: