Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
CGJ-Slide4 first

The following slide highlights the evaluation differences in the C, CGA, and CGJ Series. CGJ is TDK’s higher reliability MLCC family. It has AEC-Q200 and select MIL-Standard performance guarantees. As a reference point, 100% of each means every capacitor is selected for a particular test. Sampled indicates there are only “n” pieces selected for a given test. Qualification verifies that a particular test is performed once per year.

PTM פורסם ב: