Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Product List
Heat Shrink Micro-Molded Slide 1

Welcome to the TE Connectivity (formerly Tyco Electronics) Micro Molded Heat Shrink Boot product training module. This presentation will discuss TE Connectivity's Heat-Shrinkable product line which has been in and around the Aerospace and Defense industry for over 40 years and is recognized worldwide. The performance of TE Connectivity's heat-shrinkable products is backed by a history of proven performance, reliability, innovation and superior quality. All of the heat-shrink products are offered in an expanded form. Once the part is on, the application heat is applied to shrink the part onto the application. The pre-determined size and shape provides a tough, protective covering for the components over which they are installed.

PTM פורסם ב: