Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
HDO4096-Slide14

HD4096 technology also improves measurement precision. The peak to peak measurement of this signal shown here is displayed as 165mV by the 8-bit oscilloscope, the same measurement on the same signal captured by the 12-bit oscilloscope is displayed at 134mV.

PTM פורסם ב: