Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
PAS-Slide3

A key feature of the power analysis software package is a new power-specific user interface that walks the user through the proper setup for the measurement at hand. Inputs are selected and configured using the Input Settings tab. There, users may choose the analysis type as well as the desired tests and measurements for display. There are also shortcuts for the display of statistics and histicons. For simplicity’s sake, all measurements have appropriate power-related names such as switching losses, conduction losses, and off-state losses. The method of calculating conduction loss may be chosen depending on the probe setup.

PTM פורסם ב: