Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
CC3100-CC3200 SimpleLink Wi-Fi Slide 14

The CC3100 and CC3200 contain the same radio, so everything about the CC3100 network processor applies to the CC3200 network processor. The CC3200 is a full system on a chip (SoC) with an ARM cortex M4 and 256 KB RAM. It has several peripherals, such as SPI, UART, I2C, 4 channel ADC, and a parallel camera interface.

PTM פורסם ב: