Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Battery-Mgmt-Pt3-slide7

Here is one example that shows a benefit of using a switch mode charger even at somewhat lower current levels. Consider a USB-port charging source that could be limited to 500mA output. For example, if designing with a battery with a capacity of 1000mAH, theoretically it could be charged up to a 1A rate if the power was available. With the USB port current limit however, this isn’t possible. If a linear charger is used, then the cell can only be charged at 500mA as limited by the source current. However, if a high-efficiency buck converter is used then the battery can be charged with 600 – 700mA current for much of its charging cycle, which allows faster recharging whenever possible.

PTM פורסם ב: