Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Topic 5 The Analog Subsystem Slide 13

The ADC2 pin connections are basically identical to ADC1. It has the three comparators, three DACs, the same type of converter, and the same pin connections externally. Compared to Piccolo, the naming conventions have changed on the AIO, and the naming conventions have changed on the comparators, but the structure is essentially the same and there is the same level of functionality.

PTM פורסם ב: