Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
MSP430 Design Tools Slide 6

The eZ430-RF emulator board includes a USB connector and the circuits required to interface the development IDE software and USB port to the MSP430 target. Some key components on this emulator include a TUSB3410 for the USB interface, a TPS77301 for 3.3V regulation, and an EEPROM used for non-volatile information. The eZ430-RF provides a regulated 3.3V to the eZ430-RF2500T target board. Also, on the backside of the eZ430U, a MSP430F169 is used to accelerate the interface to the target. Additionally, ESD protection components are also used.

PTM פורסם ב: