Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
MSP432 Microcontroller Platform Overview - Part 1 of 12 Slide 5
To elaborate on the ARM instruction set, users will see that the Cortex M4F includes a full ARM instruction set, compared to M4 or M3 or M0+. This allows customers to perform operations more efficiently. Also, a Cortex M4F will process fixed point operations twice as fast as an M3 and floating point operations over ten times faster than an M3.
PTM פורסם ב: