Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
LM5113-Slide15

Additional demonstration boards have been built using the LM5113 driver from Texas Instruments and the EPC eGaN FETs. The LM5113LLPEVB is a Non-Isolated Buck converter for 48V to 10V conversion at 10A. Here the EPC2001 eGaN FET / LM5113 solution is compared at 800kHz versus a MOSFET solution running at 500kHz. You can see how the eGaN FET solution completely enveloped the MOSFET solution.

PTM פורסם ב: