Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
LM5017 Synchronous Buck Converter and COT Slide 11

As with everything else in life, there are always trade-offs that must be made. The trade-off with the COT devices is that ripple is needed on the output voltage, and on the feedback pin. This is required because there is basically a comparator in the controller, and that comparator needs some overdrive. Therefore it is mandatory to have some ripple voltage on the output, and the ripple voltage must be proportional to the inductor current. The easiest way to accomplish this is to add a resistor in series with the output capacitor. This will add the ripple that is needed for the regulation, but it is also going to have the undesirable effect of having some quantity of ripple on the output voltage. Plus the ripple will have some variation. The amount of variation will also affect, to some degree, the regulation response or the DC response as well.

PTM פורסם ב: