Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
NexFET MOSFET Technology PTM Slide 9

So what is inside the Power Block? On the left hand side, a 3D figure of the power block is shown. The low side and high side FETs have been stacked into a 5.0 mm x 6.0 mm package. The 3D image shows the low side FET on the bottom, the high side FET on top as well as a switch node clip between the two MOSFETs. The Vin clip is then stacked on top of the high side FET. The source-down stacked die helps reduce total source inductance.

PTM פורסם ב: