Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Power Management for Energy Harvesting Slide 20

The next point deals with the ability to efficiently extract energy from the source. Different harvesters have different requirements, whether it be matching the impedance, converting the AC source to DC, or tracking the maximum power point, as in solar. An efficient interface which can maximize energy extraction from the source is needed. It does little good to optimize the power converters from 85% to 95% if the interface is not carefully designed. An efficiently designed interface can extract much more power than a poorly designed interface. Next, the energy storage element must be managed. In the case of thin film batteries, they can be destroyed if they are over-discharged, so an accurate undervoltage (UV) detector is critical. Most lithium-ion technologies can create safety hazards if overcharged or exposed to extreme temperatures.

PTM פורסם ב: