Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
SIMPLE SWITCHER Power Modules Slide 9

The SIMPLE SWITCHER® power module family is the first in the industry to offer radiated and conducted EMI compliance as a standard feature. The complete portfolio of power modules complies to CISPR22 Class B Radiated and Conducted EMI standards. Low EMI enables easy PCB design because the designer does not have to worry about adding extra filtering to ensure that the end product passes. By using the SIMPLE SWITCHER® power modules the designer has plenty of margin to complete the rest of the design, so the whole system can meet the EMI standards easier.

PTM פורסם ב: