Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
TPS92070 Offline Dimmable LED Lighting Driver Controller Slide 12

This is a very short demo of two instances of TPS92070 usage. The first example is three drivers being controlled from one dimmer and the second is a single driver from one dimmer. Key points to note from these examples are the uniform changes in light output and the absence of flickering from the LEDs. To summarize, the TPS92070 is an excellent solution for dimmable LED driver applications.

PTM פורסם ב: