Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Simple Switcher Portfolio Overview Slide 6

This graph shown here represents the simple switcher step-down module portfolio. The red blocks indicate that these devices can be used for the 3.3/5 V rail. The green blocks indicate that these specific power modules can be used for the 5 and 12 V rails. The blue blocks indicate that these power modules can be used for the 24 and higher voltage rails. TI has one of the most comprehensive power module portfolios in the industry.

PTM פורסם ב: