Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
addl reverse
Some Toshiba load switch ICs include reverse current blocking. Unlike MOSFETs, which can suffer from significant leakage through the body diode, load switch ICs are able to stop reverse current flow when the switch is reverse biased. This is very useful in cases where there are multiple power sources and the designer wants power to flow only in one direction.
PTM פורסם ב:
PTM Updated on: 2017-07-10