Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Photorelays Slide 8

The new TLP32xx Series features lower capacitance and on-state resistance than previous devices. They offer CxR values of 10 to 2.5 picoFarad Ohm, which is approximately equivalent to reed relays. This series has been developed in response to requirements for high speed operation and high reliability. It is also housed in the industry’s smallest package, the 4-pin SSOP which can achieve a 50 devices/inch2 component density.

PTM פורסם ב: