Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List Associated Content
amp test2

The series connection shown here on the left is an Amp test. This is an inside look at the current passing though the circuit. The parallel connection is contrasted to the right; this is a look at voltage testing. This voltage example shows the circuit, but is looking on the outside of the circuit. This is a critical basic factor to understand in order to be able to use a meter effectively.

PTM פורסם ב: