Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
440 DMM-Scope Slide 13

Shown here is the set-up for measuring AC or DC milliAmps. Turn the selector dial to the milliamp position and connect the test leads to the input jacks. Touch the test leads to the device under test. The amount of amperage is shown in the digital display and the graphical display shows the amperage waveform. Switch between DC and AC microAmps using the keypad.

PTM פורסם ב: