Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
TMC5062 Dual Stepper Motor Slide 14

Sense resistors are susceptible to ground differences and ground ripple voltage as the microstep current steps result in voltages down to 0.5 mV. The sense resistor layout is also sensitive to coupling between the axes. The sense resistors should not share a common ground connection trace or vias, because PCB traces have some resistance.

PTM פורסם ב: