Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
How to Select a UPS System Slide 8

Also, do not be misled by a power supply that lists dual voltages and amps. Do not combine the two VA ratings, use only one. One amperage rating is for when the power supply is used in low voltage, the other rating is for when the power supply is used in high voltage. As voltage increases, amperage decreases in proportion, so the VA ratings should be similar (with only minor differences due to rounding).

PTM פורסם ב: