Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
LTSPICE-Slide16

Another available feature that might be useful is to obtain the external temperature variation input from an PWL source (allowing live measurements). A real ambient temperature profile can be measured in case of a fire starting and this profile can be applied to the circuit in the form of this Piecewise Linear source. The response time spread of the thyristor triggering can be evaluated in such conditions and is shown by the green curve in the third pane.

PTM פורסם ב: