Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List Associated Content
Simulation Example

Outlined here is another simulation where a capacitor is repetitively charged through a PTCEL. If the designer includes the ambient temperature in the simulation parameters, it is possible to see its influences in the delay time for the PTC switching to a high resistance and temperature. This exemplifies how the ambient temperature influences the repetitive charging or discharging of a capacitor through a PTCEL to a defined voltage level. Principal arguments which are sometimes used by SPICE detractors are that the temperature behavior and the IC production tolerances are not properly considered; however, it is clear that the LTspice® PTCEL models bring a decisive counter-argument to these assertions.

PTM פורסם ב: