Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Ambient Light Sensors Slide 9

The second job of an ambient light sensor is to match the human eye’s relative sensitivity which peaks at around 560 nm. Vishay’s ambient light sensors do a very good job with peak wavelength sensitivity of between 540 nm and 570 nm. The light current output shown in this table will be used in the next slide to determine the ratio of incandescent to fluorescent light.

PTM פורסם ב: