Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
prox sens2
So, what is low-power about the VCNL36687S? The maximum forward current of the pulsed VCSEL is 20 mA. With that, the sensor has a range of 20 centimeters or 7.9 inches. Compared to the VCNL4040 and VCNL4020, the VCNL36687S has comparable range at one tenth the current.
PTM פורסם ב: