Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Image of Vishay Opto VOMDA1271T Automotive Photovoltaic MOSFET Driver - Key Performance Parameters

The graph here shows the voltage generated by the photovoltaic detector. At 20°C and a forward current of 30mA, the output voltage is approximately 9V, and at 10mA it is 8.4V. This output voltage varies with ambient temperature and the input or forward current of the emitter. At 20°C and a forward current of 20mA, the turn-on time is 32 microseconds and turn-off time is 80 microseconds. Additionally, the VOMDA1271T is qualified to the AEC-Q102 automotive standard.

PTM פורסם ב: