Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
part 1
Many thermal systems benefit from the addition of vapor chambers; especially when heat sources are dense and the final heat exchanger is much larger, so the heat from the source must be spread to a larger area. Computer applications, such as processors, graphics cards and other chip-sets, have high thermally dissipated power in a small area. Fan heat sink combinations used in these applications can offer high-performance dissipation to the ambient, but much of the battle is to spread the heat to the heat exchanger with as little temperature change as possible. Vapor chambers excel at this and can transport large heat loads from small areas with very little temperature difference.
PTM פורסם ב: