Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
PCB Connector Technology Slide 3

Connection styles for discrete wiring generally fall into one of three types of technology:  screw, crimp, and spring connections. Screw connections, as the name implies, utilize a screw that is tightened to retain the wire after insertion into the connector or terminal. With a spring connection, the wire is held in place with the tension created by metal formed to provide a spring like mechanism. With both screw and spring connections, the prepared wire, either stripped of insulation or stripped and a ferrule applied, is inserted directly into the connector, terminal, or other device. Crimp connections require a separate contact be applied to the prepared wire. It is typically this separate contact that makes the connection. Each connection technology has different sub types as shown in this slide.

PTM פורסם ב: